View 'ToolBox'

 

Symbol: _visu_icon_automatically_defined_tag.png

Function: This view provides the elements that are usable in the editor. The individual elements are provided with certain identifiers in order to be able to group them. There is a button for each identifier. The elements of selected identifiers are displayed with thumbnails and can be dragged into the editor. Apart from the standard identifier, you can also define your own. You can change the size of the thumbnails with the sliders and a full-text search for element names is possible.

Call: Menu bar: View ‣ ToolBox

Requirement: A visualization is active.

_visu_img_toolbox.png

See also

Tool bar with commands

Symbol: _visu_icon_tag_selection_type_single.png

Only one button can be selected.

Symbol: _visu_icon_tag_selection_type_multiple.png

Several buttons can be selected.

Symbol: _visu_icon_manage_tags.png

The Manage identifiers and entries dialog opens.

See also

Buttons for selecting element categories (identifiers)

A button labeled with the associated identifier is displayed for each defined element category. A selected button is shown in green.

Shift+click a button

Changing the selection of the identifier and the selection type (single or multiple choice possible).

Right-click on a button

Context menu appears.

Context menu of a button

Hide identifier

Removes the button. The identifier is then invisible.

Activate identifier

Button turns green and the identifier is activated irrespective of the selection type.

Deactivate identifier

Button turns green and the identifier is deactivated irrespective of the selection type.

See also

Selection of visualization elements

The visualization elements are offered as thumbnails and labeled with name. The selection depends on the search query in _visu_icon_searching.png or on the selec­tion of the buttons.

Slider

_visu_icon_scrollbar.png 

To change the size of the thumbnails.

_visu_icon_searching.png with input field

For a full-text search by element name among all available elements

<number> Entries

Number of entries of visualization elements that are currently offered by the selection of buttons or due to the search query in _visu_icon_searching.png.